Part Number: TPS566235
Dear *,
is it possible to have more capacitance on the output of TPS566235 than is described in Table 3 page 16 of DS ( 110uF) ?
How is the mAX capacitance Cout calculated?
Best Regards,
David.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, David
110uF is TI recommended MAX Cout.
You can use the bigger Cout, but please note:
During soft start, the Vout is a linear ramp up which requires a constant charging current I = Cout * Vout / Tss, this current is called inrush current, usually, it should be smaller than 1A, so we can calculate the max Cout is 1A*1mSec/Vout.
However, TPS566235 has very good load transient performance, it doesn't need very large Cout, i think Cout=110uF is enough for majority application.
Besides, 110uF has been validated by TI.