This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How Can i design Solar powered AA battery charger and Battery level monitor with Tiva C

Other Parts Discussed in Thread: EK-TM4C123GXL

Dear experts,

now i am working with EK-TM4C123GXL and now i want to power up the device with AA rechargeable batteries and also i want to charge the batteries with 12v Solar panel or 12v adapter, i don't know to how to design the circuit for that. then i want to monitor the battery level with my controller which is connect or power up by the battery.

Solar panel details:

Voltage at Pmax - 17.3V

current at Pmax - 0.57A

open circuit voltage - 21.0V

Short circuit current - 0.61A

Application Class - Class A

Note: Suppose if i will use this 5V Solar panel what will i do and what changes will do in above design

https://www.banggood.in/5V-10W-Portable-Solar-Panel-Slim-Light-USB-Charger-Charging-Power-Bank-Pad-p-1297325.html?rmmds=search&cur_warehouse=CN

thank you