This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25119: Output Unstable

Part Number: LM25119


Dear Team,

The customer using LM25119 for 18V/120A application.

They have 2 board with the same schematic, but slightly different layout.

One board work properly till 100% load, but one of the board will unstable around 90A.

Do you have any comments on the schematic may improve the stability?

Inductor:

Waveform:

BR

Kevin