I am trying to validate the functionality of the LM5069 chip using the evaluation board. I tested the board as is first, and reached the correct cutoff of 2.5A. I need a current limit of 9A, so I switched R5 to 5mOhms, but this resulted in the board getting too hot with the power FET that was originally on the board. I switched the FET to be able to handle more current and power, however, the board is still getting very hot. Is there enough heat dissipation on the Eval board to accurately test at this amperage or is there a recommended method of heat dissipation for the chip and FETs