This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS259827ONREGET dos not power up with load

Other Parts Discussed in Thread: TPS259827LEVM, TINA-TI

FYI the part  I am writing about was not recognized in the above Part number search:

 I am planning to use several “TPS259827ONREGET” for the engineering run I have purchased and using the TPS259827LEVM eval board

The main issue right now is : When the load is applied before powering up the output does not come up but if no load is applied on power up and the load is applied after  no problem I played with the different jumpers that might affect this issue: Output Slew rate control, current monitoring , programmable fault monitor and current limit.

System configuration: Input voltage is 10-19.5V, max current 6A load.