Hi Team,
I am using the Overcurrent protection device PN: TPS25942L
I am using the IC also to measure current V/A (on R235 for example)
However I found that I get a DC voltage in the Current sense output even the load is Zero
I try to calibrate the DC-DC but it acts like a noise flor of~40m-100mV on the IMON output
I wonder if there is a way to improve the measurement on low currents <100mA?
Can you recommend on another IC which can measure low current <25mA too? (preferred to be pin compatible/same footprint)
Please advise.
Thanks,
Shlomi