Other Parts Discussed in Thread: TPS1H100-Q1, TPS2H160-Q1
I'm currently using the TPS high-side switch to control a 10W (1.667A@ 6V) tungsten lamp, but new requirements of a 20W lamp (3.25A@6V) exceed the current limits of the device. Can these parts be effectively used in parallel? I don't find anything in the datasheet to encourage or discourage this practice, and would think that MOS thermal effects would be such that the parts would share current well. But I question whether the protection circuitry built into the device would detect conflicts during switch-on. Obviously, the parts would need to be set up identically and switched from the same source, but there may be other issues involved that cause problems.
thanks for your thoughts,
Rob Valley