Hi
I think I use LM5155 under Vsupply=48V, Vbias=Vcc=15V and Vout=16V.
May I use this device under this condition?
Best regards,
Yokota
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Hi Yokota-san,
Thank you for considering the LM5155 in your system.
Yes, you can tie Vbias and VCC together at 15V, but you must make sure that your FET gate voltage can handle the required voltage. However, I would recommend you to lower the Bias and Vcc voltage rail to 12V if it is possible so that you are not so close to the maximum rating pin.
Additionally, Vsupply must not be connected to the bias or vcc pin because you will violate the absolute maximum voltage rating.
Thanks,
Richard