Hi,
I intend to use LP8556, but I would need further information about correct usage of the device.
I would need to poweroff some stuff around for deeper low power mode, but I can' figure out some stuff in the datasheet.
- In Functional Block diagram @ page 12, a POR appears, but there is no other information about this. What are the electrical settings of the POR?
- Can the device have a EN/VDDIO greater than VIN ( min = 2.7V).
- Can it work it EN.VDDIO = 3.3V and VIN=2.7V?
- What if EN_VDDIO = 3.3V and VIN = 0? Is there any risk?
- If VLDO falls below POR level, is the device reseted by the POR (µcut)
Thanks.
BR