Hello Jeffery,
The ADP125A is an LDO, and the ADP2300 is a non synchronous buck converter.
These are supported by different TI teams, so I will split this thread after this reply and route to the 2 teams.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Unfortunately we do not have an LDO exact P2P. The current best option would be TPS735 in the SON-8 package.
TPS7A90 would be the next best recommendation as it is in a SON-8 package except 2.5mm x 2.5mm not the 3x3.
TLV758P would also be a solid option and is next-generation of TPS735 in a smaller 2x2 package.
regards,
Wilson