This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS549A20: Soft Start and PGood timing

Part Number: TPS549A20


Hello E2E,

I want to confirm a few questions about the TPS549A20:

Soft-start:

Per table 12, the default SS time is 1ms, correct? 

What is the min and max? 

Pgood:

The default PGood time is 1ms, correct?

What is the min/max on this spec? It appears that this closest data in the electrical characteristics table shows min; typ; max as 0.819; 1.024 ;1.228.  Would I be safe using those as the default min/max values?

Thanks!

Russell