This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS745: TPS745-Q1 adjustable output option

Part Number: TPS745

Hello,

Can you please confirm or clarify the following about the TPS745-Q1 adjustable option?

  1. TPS74501-Q1 is the base part number for the adjustable output option with AEC-Q100 qual.
  2. TPS745-Q1 advance info datasheet does not have info on the FB resistor divider selection considerations. Is it valid to refer to the TPS745 Datasheet Rev A, section 8.1.1 (pg. 17)?

Thanks,
Alan Ocampo
Analog Field Applications
Texas Instruments Inc.

  • Hi Alan,

    1. TPS74501-Q1 is the base part number for the adjustable output option with AEC-Q100 qual.

    TPS74501PQWDRVRQ1 will be the adjustable option.

    1. TPS745-Q1 advance info datasheet does not have info on the FB resistor divider selection considerations. Is it valid to refer to the TPS745 Datasheet Rev A, section 8.1.1 (pg. 17)?

    Yes, it's valid to the automotive version as well.

    Regards,
    Jason Song