Hi team,
The d/s describes that the LED current can be programmed by varying VIADJ between 140 mV to 2.25 V. Does the range of 140mV to 2.25V include tolerance? If not, could you let me know the min/max range? ( For example, this range needs to be considered +/-10% tolerance, so the range will be 154mV(min) to 2.025V(max).)
Regards,
Yamaguchi