Part Number: TPS61500
I have built a circuit similar to the TPS61500EVM board. Schematic is attached with this.tps61500evm-schematic.pdf
The problem with the circuit is, current flowing through the LED is very less with the following components:
Rfb = 0.22ohm
Vin = 5 to 9V
OVP set to 13.5V (100k and 10k)
Vf (LED) = 12V
I (LED) (max) = 1000mA
Also the voltage at pin FB is never 200mV. It is always below 120mV. Is is because of the compensation capacitor? Or is there anything wrong with the circuit?
Thanks in advance.
Regards,
Sudheendra H