This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25120: watchdog timer reset device despite I2C read/writes every second (interrupt driven)

Part Number: BQ25120


I have the BQ25120A in a board and am having a lot of difficulty with it.  First I need to address the watchdog timer, which is resetting the device every 50 seconds despite my conducting I2C reads every second (interrupt driven).  This transaction is rated "NRF_SUCCESS" by the NORDIC '840 firmware so I believe it is actually happening.  There are other issues but I need this one solved before moving onto them.