This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40200: Absolute Max vs. Recommended Max

Part Number: TPS40200


The TPS40200 datasheet indicates that the abs max input voltage is the same as the recommended max input voltage = 52V.

This is unusual- typically absolute max is some amount greater than recommended max.

Is this a typo or is the data sheet accurate?

  • Hi Antenna Head,

    Yes this unusual, but can be found in older generation devices. I went and looked at the first revision datasheet and it shows the same recommended and absolute max input voltage so I believe this is not a typo.

    Regards,

    Ethan