This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Thank you for posting. A Schottky does does not prevent the issue, because the pin can still be pulled to one diode drop above GND. The transistor prevents it from becoming >0V. So, the safe approach is to use a transistor as shown in Figure 30. It just requires a small signal transistor. By the way, the substrate diode spec is not available, as we do not characterize parasitic devices.
Thanks,
Youhao Xi, Applications Engineering.
Hi Dai,
Thank you for understanding. What you really need to know is the worst case min Vf of the substrate diode, which is why we cannot specify to allow you to have a safe selection of the external diode.
Best Regards,
Youhao