This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25570: Solar Panel

Genius 5355 points
Part Number: BQ25570
Other Parts Discussed in Thread: SM74611

We are using BQ25570 and got some failure cases BQ25570. 

This is circuit diagram of BQ25570:

Figure 1: 

1. Connect Solar Panel 5V, 2.6W to BQ25570. 

2.BQ25570 to Battery(4 cellx 18650 parallel) 

3.BQ25570 to Diode (SM74611) to  Load

Figure 2: 

1. Solar Panel Spec

Issue:

The battery voltage drops very quickly (voltage value ~ 0-1V) and the resistance from VBAT pin to GND is ~ 40 Ohm. 

2/4 devices encountering this case is in storage state (not yet put into actual operation), so Solar charger feature not yet active. 

- The power of Solar Panel is larger than the input power allowed of BQ25570, but 2/4 devices are in storage state and I had a small test is using Solar Panels 9V & 12V for the input of BQ25570, the result is BQ25570 still works normally 

- Quality of Battery is not good ( internal resistance of Battery is of large value) so it affecting to IC operation

- Activity characteristic of the Diode cause this case 

Please kindly advise.  

We are connected a 5V, 2.6W