Other Parts Discussed in Thread: EV2400, , GPCCHEM
Dear Sir,
"Error: [RUP_DIS / RDIS: Not Clear]" is displayed after Start Re Relax in the learning cycle.
what is the cause?
■ Test conditions
・ Read ggfile (ggfile for our battery tested by TI + change of various parameters)
・ Testing Learning Cycle in Automated Mode (Connect EV2400 and evaluation board via FET)
■ Attached data
1: 00_190717_Learning_pretest_RUP_DIS_Error.log (1st Learning Cycle exam log)
2: 00_190718_Learning_pretest_RUP_DIS_Error.log (2nd Learning Cycle exam log)
3: 02_N4HPGMA00001-bq27426G1-LC1202_190712.gm.fs (gg file used)
4: 00_190717_Learning_pretest_Status.txt (1 Status log)
190718_BQ27426_Learning_Cycle.zip
■ Remarks
・ In the test of 1 and 2, Opconfig D (23 ⇒ 2b) and Update Status (00 ⇒ 03) are changed.
・ I changed OpconfigD because ChemID of OpconfigD remains 3230 even if it is changed from 3230 to 1202 in Chemical.
■Reference
The following E2E thread was referenced (searched by "RUP_DIS").
Best regards,
Chiaki Endo