This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3703-Q1: threshold accuracy

Part Number: TPS3703-Q1


Hello,

my customer is currently working on a new project and they plan to use the TPS3703-Q1 device (TPS3703A4120DSERQ1 and TPS3703A4330DSERQ1). However he as question regarding the specified threshold accuracy in the datasheet. We specified ± 0.7% for -40°C to +125°C. The engineer wants to know if we can provide typical threshold accuracy values (other than the curves in chap. 7.7 of the datasheet) for the temperature ranges -40°C bis 85°C and -40°C bis 100°C?

My understanding is that this would be ± 0.7% since the ranges he mentioned are all in the-40°C to +125°C. Is my understanding correct?      

Best regards,

Stani