This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65132S: Difference between -S and -B0 version

Part Number: TPS65132S


Hi team,

Looking at the datasheet, the difference between -S and -B0 are as follows. Is there any main difference between both devices?

1. -S version can output up to 150mA by setting HIGH to SYNC-pin.

2. -B0 has enable pin for each rail (ENN/ENP). -S has enable pin for both rails(EN).

3. -S version only has DLYx register.

4. Soft start time (-B0 : Fast, -S : Slow)

5. Discharge behavior is different that described in Table 2.

Regards,

Saito