Hello
I have a question about UCC28180.
Question 1
The PFC (UCC 28180) was turned off from the on state using the measurement power supply. At this time, the potential of the following terminals of UCC28180 is temporarily reversed.
Do you need any measures in this situation?
Also, if it is necessary to take measures, is it better to connect a diode from VSENSEpin to VCCpin?
<On the potential>
・ Measurement power ON state: VCC> V SENSE
? When switching the measurement power supply from ON to OFF: VCC <VSENSE
Thank you.