Other Parts Discussed in Thread: TPS62147, TPS62148, TPS62140, TLV62084, TPS62065
Hi All,
My customer is designing an application for which they need to deliver prototypes by the end of August.
It is a battery-powered product.
Customer doubt regards battery configuration.
I could work at 3.6V directly without anything stabilizing this voltage or working at 7.2V and then inserting a dcdc switching.
On the one hand the 7.2V would protect me from critical situations such as temperature (the 3.6V would not be guaranteed), on the other hand customer has no margin on the component cost to add components.
Furthermore, the product is critical in terms of consumption.
TLV62150 is a good option as dcdc switching also becasue of very low 19uA quiescent current.
The problem is the component cost @50ku/yr.
Or would you have alternatives to propose for lower cost solution fitting the above requirements?
Many Thanks,
Antonio