Other Parts Discussed in Thread: TIDA-00449
Hi team,
My customer is using BQ76930 for 6S li-on battery in their design and have some questions as below:
1.In the EVM board, there is a MOS between C10 and REFSRC, why we need the MOS here? Could they connect the REFSRC to the third or fourth cell instead of C10? By the way, why put the C4(1uF) cap in this place? Would all the voltage from C10 add to the C4 and cause some issue when the MOS turn on?
2. What's the use of D4 and D6?
3. Why VC5X need C12 to VC5B, and C9 to VC6? Is it because VSS and VC5X is two reference "GND" here? How does it work internally?
Let me know if you have any suggestions, thanks.
James