This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H100-Q1: High speed current sensing

Part Number: TPS1H100-Q1

Dear team,

Is it possible to sense 40kHz to 50kHz PWM current?

Datasheet says "only up to 2kHz" and I see tough "timing requirement - current sense", but that case just describe depending on input ON/OFF signal.

What if IN is always turned ON and output switch with 50kHz by external switch? Can TPS1H100-Q1 sense it?

Thank you.

Regards,

Oliver Kim 

  • Hi Oliver,

    If you are leaving IN high and externally PWMing the output, TPS1H100 should be able to sense the current variation and report it through the CS.

    Do note that the sense waveform will be complicated because of the the fast switching and parasitics of the system.