Other Parts Discussed in Thread: PMP8606, UCC24612, UCC28951, UCC21520, LMG1020, UCC27611, LMG3411R050, LMG3410R050, PMP20657
Hi Team,
My customer is considering to use UCC28950 for the following application by placing it on the primary side.
- Phase-Shifted Full-Bridge application
- UCC28950 on the primary side
- Secondary synchronous rectification is done by another controller
- VIN: 300V typ
- Vout: 15V typ
- Iout: 150A max
For the primary side application, I showed the PMP8606 to them as reference.
For the secondary side application, they want to use a Synchronous Rectifier Controller IC because of high output power.
Q1. Are there any concerns to use a external Synchronous Rectifier Controller IC in the secondary side compared with the synchronous rectification feature of UCC28950 inside?
Q2. What is the recommended Synchronous Rectifier Controller IC for this kind of application?
How about the UCC24612 High Frequency Synchronous Rectifier Controller?
Q3. If GaN FET was used for synchronous rectifier switching device, are there any guidelines to use it?
Thank you.
Best Regards,
Koshi Ninomiya