Hello TIer,
We're test input cold crank as below test waveform now.
Spec is input from 9V to 16V and output 31V / 260mA use TPS92692-Q1 designed boost topology.
We need qualified Td 100us / 300us for DRL mode and PL mode. Currently PL mode have flicker in 300us.
Do you have any recommended can suggest to me? thanks!
fine tune step us below.
1. Oringenal RC config as below schematic. test result is DRL/PL mode are failiure in 300us.
2. Final RC as below and DRL can qualified 300us except PL mode.
C39 30nF
R17 9.1k
C29 1nF
C30 10pF
R19 removed
R12 0.1
3. Base on step 2. Increase and decrease input / output capacitance, the test still failiure in 300us.
Test Waveform
Part of Schematic