This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: Can LM5175 take in Vin = 3.5 ~ 24V to generate 5V 30A output ?

Part Number: LM5175

Hi 

Can LM5175 take in  Vin = 3.5 ~ 24V to generate  5V 30A output ? 

thanks!

  • Hi PY,

    According to the datasheet, its VIN operating voltage can be as low as 3.5V.  So, the answer is yes.  If you need a ref design, please make a request to the PDS group.

    Thanks

    Youhao Xi, Applications Engineering.