Other Parts Discussed in Thread: LM5023,
We make a AC to DC power module, mainly used in portable chargers, and plan to have LM5026MM to do it. There is a TI schematic diagram in the annex. There are several confusing places to ask, what is the output power of 1. +24V+15V-15Vl? 2. Can + 24V be changed to 5V 1A? 3. I need to make an AC to DC, three-way output, - 15V 100mA + 15V 100mA how to change the circuit and transformer, have good suggestions, thank you!