Hello
My customer finished their design using TPS92518 ( already in mass production ) .
Thank you for your support so far.
Now customer intend to add smaller ILED product-line for ILED is 300mA at 100% brightness.
( So far, ILED is 1000mA )
They hope to have without H/W design change.
Customer want to have just change LEDx_PKTH_DAC register only and tested in their product actually.
Condition:( schematic is also same as EVM)
* LEDx_PKTH_DAC = 102 ( changed from 223 to 102 in order to adjust from 1000mA to 300mA max at 100% brightness.)
* LED_TOFF_DAC = 45 :no change from 1000mA case
* switching frequency is almost 320KHz :same .
* inductor: 330uH TZSH12080-331(DSC):same
* shunt FET dimming is used. So, cap with Inductor ( EVM manual* C18/C17) are removed and 0.1uF are inserted in place of those as EVM.
www.tij.co.jp/.../sluubm0c.pdf
Issue
ILED is changed depend on duty ( 304mA ~ 318mA) if VIN is high.
VIN=55V
ILED=318mA@VF=8V
ILED=309mA@VF=26.5V
ILED=304mA@VF=45V
VIN=24V: no problem
ILED=301mA@VF=8V
ILED=300mA@VF=13.5V
ILED=299mA@VF=19V
-----
On the other hand, when ILED is 1000mA, no problem found.
VIN=55V
ILED=1003mA@VF=8V
ILED=999mA@VF=26.5V
ILED=996mA@VF=45V
VIN=24V
ILED=997mA@VF=8V
IL ED=996mA@VF=13.5V
ILED=996mA@VF=19V
------
Inquiry ( please have your comment)
I think inductor magnetic energy is too much for stable control in case duty is too small/ and ILED is small (300mA) for TPS92518.
To reduce frequency ( bigger LED_TOFF_DAC ) seems to be corretive action, but I am not confident with theoretically.
Customer had also tested and to reduce frequency (320KHz to 250KHz) with LED_TOFF_DAC = 45 to 50 seems corrective action....
Customer want to know the mechanism in theoretically, but would you please advise your opinion about the mecanism ?
We know VCSPx-VCSNx peak current threshold tolerance is good when LEDx_PKTH_DAC.( But seems no relationship to duty..)
Do you recommend to have LEDx_PKTH_DAC = 223 or something ( bigger ) and change shunt resistor?
Best Regards