This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2388: Pin22 connection

Part Number: TPS2388

Hi,

Can we connect pin22 to 3.3V?

Does it have any effect?

  • Hi User!

    Per the TPS2388 datasheet Section 5, we recommend leaving the pin open.

    A link to downloading the datasheet can be found here --> http://www.ti.com/product/TPS2388 

    However, connecting a 3.3V signal to pin 22 will not damage the IC. If the 3.3V signal is noisy, it may couple to adjacent pins and cause unusual behavior with the TEST1 pin (pin 23). It should not have major effects on the operation of the device, but we can't be sure as we haven't tested our device in this configuration.

    Thank you for reaching out to us today and don't hesitate to let us know if you have any more questions!

    Aidan

  • Hi User! 

    Did the information I provided about Pin 22 of the TPS2388 help you to make a decision regarding connecting it or not? If so, please mark this resolved to let us know! 

    Thank you so much! 

    Aidan Davidson