Other Parts Discussed in Thread: GPCRB
Dear Sir,
Please confirm the following question.
1. When is the FCC updated?
2. In our products, SOC jumps (5 -> 0%)near the end voltage (3.3V). What should I do to avoid jumping (5 -> 4 -> 3 -> 2 -> 1 -> 0%)?
3. Is there any way to check which measurement algorithm is detected as DISCHARGE, CHARGE, and RELAXATION (for example, flags etc.)?
4. Current consumption of our products is as follows.
190724_Consumption current.xlsx
How much value should I set the current threshold and the relax time?And do peak currents affect the detection of each relaxation mode?
Best regards,
Chiaki Endo