Dear !
BQ24171: Battery off and on charging when at chargering current is about 300mA near end,the STAT led blinking error,
Pls help,TKS!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear !
BQ24171: Battery off and on charging when at chargering current is about 300mA near end,the STAT led blinking error,
Pls help,TKS!
Hi,
Does the blinking correspond to the charger going into and out of termination or does it blink a constant frequency? Can you send a scope short showing STAT, V(BAT) and I(BAT)? If you have a highly resistive connection to the battery then it is possible that the 300mA charge current is artificially raising the battery voltage to termination. Then, when the current goes away, the battery voltage droops below the recharge threshold.
If blinking is constant frequency independent of charge current then it is one of the errors below:
Charge suspend - what is the input voltage at PVCC relative to V(BAT) voltage near end of charging?
Input overvoltage - unlikely
Battery overvoltage - possible if large transients on system are causing supplement through BATFET diode
Timer fault - what is the timer set per TTC pin?
Regards,
Jeff