Other Parts Discussed in Thread: TPS546C20,
1,We are using TPS546C20 to design DCDC power supply, the input is 12VDC, the output is 5V70A, and the staggered design is adopted. Now the test only has 5C25A current output. In the test, the more current will be protected. UVW protection will occur. Please confirm the problem. How can I debug it. I use the EVM test of TITPS546C20AEVM2746 to test 0.9V70A test. When I change the parameter to the output is 5V, the load current with load can only be brought to 26A, which is the same as the board test result I designed. The attachment is the data of my SCH and test verification
2,How does TI's TPS546C20A tool export register addresses?12V-5V D2D.pdftps456c20a.docx