Other Parts Discussed in Thread: AM4372, TPS3825, TPS65218, , BOOSTXL-TPS65218, IPG-UI
I have a design using the TPS65218 to power a AM4372 processor. I want to be able to go into a low power mode and wake up from RTC or external signal and I want my unit to always power up without having to use the push button, but my design may not always have coin cell battery attached. So I connected the CC pin to my input voltage with a resistor divider to drop the voltage to an acceptable level. I also connected the AC_DET pin to the RESET* pin of a TPS3825 power supervisor so that the AC_DET pin is pulled down on low power and then pulled up after. I tested this circuit on the first rev of my prototype and it worked as I expected. But when I had multiple units built with the changes I can not get consistent FSEAL breaking. Some boards will break FSEAL and some boards won't..