Other Parts Discussed in Thread: BQSTUDIO
Hello,
we are trying to complete a learning cycle using BQ28Z610 EVM and 2S2P NiCoMn Battery pack (5200 mAh). The chem id is 0297.
As per the learning cycle document, first we updated the chemistry id.
in the advanced comm I2C, (BQSTUDIO) , we set I2C address - 0xAA, start register 0x3E, byte to write - 0x22 0x00 (to turn on the charge and discharge fets) and it reflect on data memory.
by sending I2C address - 0xAA, start register 0x3E, byte to write - 0x21 0x00 (to set the GAUGE_EN in manufacturing status register and QEN flags in IT Status register) but we observed that only GAUGE_EN is updated but QEN flag did not update automatically (for further process we set this bit manually). Updated status is changed from 00 to 04.
In the relax time for 2 hr , Some register bits (like [VOK] and [RDIS] ,REST, FC, Update status) are clear and set mentioned in the document so it is updated automatically or we need to set manually?
we set the register bits manually (in the relax time : VOK and RDIS = 0 , Charge Battery to Full : VOK = 1 before start of charge FC = 1 after battery end of charge ) and complete the cycle but we are not getting proper percentage.
I have attached datasheet of battery.
Thanks2548.18650-3.7V-2600mah specification.pdf