Dear Team
Do we have reference design with 48V adapter priority for the customer to duplicate the circuit?
Or we can only follow the below application in section 3.5?
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team
Do we have reference design with 48V adapter priority for the customer to duplicate the circuit?
Or we can only follow the below application in section 3.5?
BR
Kevin
Hello Kevin,
Thank you for your question. We do have an EVM with a 48V adapter priority: TPS2373-4EVM-758
http://www.ti.com/lit/ug/sluubj1a/sluubj1a.pdf
I have the EVM and I went to test it in the lab.
I tested the board by connecting a 58V PoE cord in the power in. Then I connected a 48V in Adapter Port, J3. I measured the voltage on VDD (TP10) and it swtiched from 58V from the PoE to 48V once it was powered. I also confirmed if there is no PoE, the board still operates on the adapter voltage alone. I also confirmed if we remove the 48V from the adapter the board still operates on the PoE alone.
The EVM has a jumper (J6) that enables adapter priority. The customer could either keep it or directly connect the ends in their design.
Does this answer your question, or is there anything else I can help with?
Regards,
Michael Pahl
Dear Michael,
Really appreciated for your help.
I will check with the customer and get back to you soon.
BR
Kevin
Kevin,
Thank you so much for getting back to me.
I will mark this post as resolved, but feel free to reach out at any point or create a new thread.
Regards,
Michael Pahl