Other Parts Discussed in Thread: USB2ANY
Hello
I follow the 7.6.8 procedure, in step 2, the 7bit address is 58h, so add one write bit "0", so I need to send B0 right ? but when I send B0 , no ack signal return
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Fandy,
Yes, please check our the hardware and make sure the I2C communication is right. I suggest to use our USB2ANY tool to test :http://www.ti.com/tool/USB2ANY?keyMatch=USB2ANY&tisearch=Search-EN-everything&usecase=part-number or you can also use our EVM board to test.
Regards
Sean