Hi Sir,
Can you refer below design spec to see if we have suitable total solution can make it?
Input Voltage: 20-100VAC
Input Frequency: 100-330Hz
Case Style: Open Frame
Size: As small as possible.
Output Rating: 12-13VDC @ 16A minimum (can be slightly derated at 20VAC input, The derating is linear from 80% at 20VAC input to 100% at 30VAC and higher input)
Thank you.
Edward Chen