This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: thermal derating at during power up with a capacitive load

Part Number: TPS1663

Hi team members.

I want to heat derate TPS1663 and use it.
When considering thermal derating  during power up with a capacitive load , can I use Transient junction temperature(165℃) instead of Operating junction temperature(150℃)?