Hi team members.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team members.
Hi,
Do you mean to use dVdT startup so that the device does not enter into thermal regulation loop during power up with a capacitive load ?
Best Regards,
Rakesh
Hello Rakesh
Thank you for your reply.
My explanation was missing.
Under what conditions should I use operating junction temperature (150 ° C) and transient junction temperature (165 ° C)?
Hello,
There are two temperature set points in TPS1663: Thermal regulation T(J_REG) and Thermal shutdown T(TSD) .
T(J_REG) is the junction temperature regulated by device at start-up if the device goes into thermal regulation due to large inrush current at start-up
T(TSD) is the junction temperature at which the device goes into shutdown due to excessive power dissipation during over load or over current condition.
For thermal calculations after power up or start-up, T(TSD) should be used.