This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5026: LM5026 excel calculator and 1/2 DC/DC brick suggestion

Part Number: LM5026

Hi Team:

Due to RD could not to find WEBENCH design  and calculator of LM5026 , could you help to provide excel calculator of LM5026 for customer request ?

As confirm with RD for 1/2 brick DC/DC isolation module series application ,if we have more better solution , please help to recommend , will proposal to RD , thanks.

RD would like to select one solution to fulfill below condition.

DC input 18~72V / output 3.3V/16A

DC input 18~72V / output 5V/10A

DC input 18~72V / output 12V/4.2A

DC input 18~72V / output 24V/2.1A

Regards / Mark

                              

 

Input:18V-72V ,Output:24V