Part Number: LM5023
Hi,
We have designing AC/dc converter 100W power supply.
input 84 to 264V AC 50hz
Output 24VDC 4.2A
Switching frequency 58KhZ
Here we facing Overload protection issue @ different input voltages.
We have place 0.1_ohm current sensing resistor.
Issue: Controller turned closed loop(overload protection)
@ 120VAC input - Output current @ 3.6A output controller turned off
@ 240VAC input - Output current @ 5.1A output controller turned off
Find the attached schematic. We need at 4.2A controller turn off the circuit at 84V - 264V input.
Kindly give the solution for this issue.
Regards,
Sathishkumar V.