We have questions about LM317A.
We check the temperature increasing.
Vin=24V
Vout=3.3V
Iout=31.6mA
PD=(24-3.3) x 0.0316
=0.65W
Increasing temperature = RΘjc x PD
= 16.2 x 0.65
= 10.53(℃)
But the increasing temperature is 28.7℃ when our customer takes measurement.
Formula and measurement result are different.
Please tell us the reason why hte formula and measurement result are different.
Is the formula correct?
Which part of 10.53℃(formula result) is the temperature?
Which parts of this IC should we measure when we want to check the increasing temperature?
Best regards,
Takahiro Nishizawa