Hello,
Iam designing a Multi rail Power supply unit with LM5155-Q1 with the following specifications.
Vin 12to13.5V
Vo=15V (4-rails) and -5V (4 rails)
Po=6.5W
primary inductance of flyback transformer is 2.5uH with turns ratios as 1:1.2:0.7
For the circuit i want to implement with primary side feedback control, with provided data sheets and application note i am not able to calculate COMP pin elements (Type-2) compensation.
Can anyone provided me the information to calculate these values
Regards,
Abhilash