This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am looking for the full part number of this Voltage regulator which will provide 5V output in response to a 24VDC input single but in the TO-92, "FORMED LEAD OPTION".
I can not find formed lead part number specs. Thank you
Hi Nehemiah,
Upon checking the datasheet, even there is a "formed lead" option, I cannot find the orderable for the TO-92 package with formed lead. Please allow some time for me to investigate this issue, and I will get back to you in 2-3 business days.
Regards,
Jason
Hi Nehemiah,
For TO-92 we have two shipment methods, one is bulk and the other is in tape. We ship the formed leads option in tape while the straight lead option is in bulk.
Unfortunately the datasheet doe snot cover this today, but a quick way of noting this is through the minimum order quantities. The larger amount of the two is the tape shipment option. This is the LM340LAZ-5.0/LFT4 which has the formed leads.