Other Parts Discussed in Thread: UCC256403
I need an OVP that has a tighter precision than can be obtained by sensing the secondary voltage with a Bias Winding. Therefore, The OVP level will be monitored by circuits directly at the Output and a separate optocoupler used to send the OVP trigger to the primary side. This signal must latch off the UCC256303 until its bias power is reset.
Is there a way to use the BW pin to do this? Perhaps couple the phototransistor thru a charged capacitor to the BW pin to drive it below negative 4V ? But the diagrams imply that gate drive pulses must be happening during the overvoltage condition in order to repetitively sample the negative voltage on the BW pin. Is that correct?
If the OverVoltage comes from an external source (rather than from a broken voltage regulation feedback signal) the feedback will stop the gate drive, and therefore the OVP sampling. Correct?