Part Number: BQ24171
Other Parts Discussed in Thread: BQ25896, BQ25601
Hi Experts,
We are testing BQ24171RGY as below conditions.
- Charge Voltage : 4.2V
- Charge current : 700mA
- Battery : Li-ion
- input current : 600mA
In this case, the supply voltage is going down then the charger stops to charge the current. After that, the supply voltage is going up and charging is resumed. This is repeated.
Basically, we are assuming to use the higher input current than charge current.
Does above behavior matter or not?
Regards,
Uchikoshi