Hi Sir
If I connect Rhi=10V / Rlo=6V
what's the accuracy voltage for each step ?
For example
10V-6V =4V
4V / 10step = 0.4
if the accuracy is 5% = 0.38V~0.4V for each step
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have notified our expert regarding this topic. Please expect a response by 8/2/19.
Thanks,
Aaron
Hello Kai,
Your description above is correct.
Please note that accuracy is specified in the datasheet at 2% but under the conditions of Rhi=10V and Rlo=0V. With the conditions, you provided (Rhi=10V and Rlo=6V), I believe assumption of 5% accuracy should be ok but please do note that accuracy is only tested at the conditions provided in the datasheet.
Kind Regards,
Liaqat