This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54531: Request a design review

Part Number: TPS54531


Hello

I Request a design review for TPS54531.

Condition

Vin : 20V

Vout : 5V

Iout : 5A

Best Regards.

  • Hi,

    The output capacitance is litter small. What is the rated voltage of output capacitors? You'd better check the real output capacitance, because there is derating with DC bias for ceramic capacitor.

    In addition, you can use Webench to do the simulation.

    https://webench.ti.com/power-designer/switching-regulator/customize/134?AppType=None&Flavor=NA&O1I=5&O1V=5&Topology=BUCK&VinMax=28.00&VinMin=8.00&VoltageOption=NA&base_pn=TPS54531&flavor=NA&lang_chosen=en_US&op_TA=30&optfactor=3&origin=pf_panel&refpage=https:%2F%2Fwww.ti.com%2Fproduct%2FTPS54531

    Shawn